Hi Team!
I want to improve speed response of acceleration and deceleration.
I re-write the value of CL_ACC and CL_DEC of CLOSED_LOOP1 register, but not work.
No speed change can be seen even if the value was re-write.
Are there any registers that need to be rewritten at the same time?
Also, is there a PID parameter for speed control on this device?
I'm using RTM devices for test.