Hello,
I was verifying the Auto-Retry mode on the OCP feature and I got these scope shots:
CH1: VM, CH2: IOUT, CH3: OUT1 CH4: nFAULT
The setup is using Auto-Retry OCP mode with an E-load trying to draw about 9A from OUT1 and OUT2 continuously.
Two issues:
1) Why is tretry around 100us in the first image
2) Why do the FETs not retry as soon as nFAULT asserts high again. There is a 486us delay between nFAULT assert high and FET conducting again