This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8343-Q1: Current Sense Amplifiers' Input Voltage Range

Part Number: DRV8343-Q1

Hello,

Input voltage ranges of DRV8343-Q1's current sense amplifiers are defined as VCOM = ±0.15 V (Max) and VDIFF = ±0.3 V (Max) in the data sheet and it gives me the impression that they are too narrow if I compare it with general op-amps.

Questions

  1. Are the specs independent of the CSA's gain or VREF divider setting?
  2. How could the CSA behave if the input ranges are violated? For example, parameters related to the CSA may get out of the specs but the CSA will continue to function, or strange behavior could appear, etc.

Best regards,
Shinichi Yokota

  • Hi Yakota-san, 

    Thanks for your question! I will try to get back to you on this tomorrow.

    Regards,

    Anthony

  • Hi Yakota-san,

    Since the sense amplifier circuitry is all integrated into the device, this introduces some limitations from a design standpoint compared to general op-amps which is why the input voltage range is more constrained than a more general op-amp.  If the input exceeds the Vcom or Vdiff spec, this can result in significant gain errors being introduced, leading to inaccurate CSA output results. While exceeding the Vcom or Vdiff spec should not damage the device as long as the abs max voltage of the pins are not exceeded, the CSAs cannot be guaranteed to work as described in the datasheet if the input voltage exceeds the specs.

    Regards,

    Anthony Lodi