Part Number: DRV8432
I supply 13V to DRV8432.
\Fault, \OTW pins Max voltage is 7v.
but i measured that pins voltage is 12v.
so, is it right operation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8432
I supply 13V to DRV8432.
\Fault, \OTW pins Max voltage is 7v.
but i measured that pins voltage is 12v.
so, is it right operation?
Hello,
Under no circumstances should /Fault and /OTW be 12V unless you have a resistor connecting them to 12V. They are open-drain outputs, so high voltage is only possible if they have been pulled up to 12V which is not correct. They need to be pulled up to a 5V or 3.3V logic supply from your microcontroller.
Regards,
Ryan