This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: SHx pins can not be HiZ in 1xPWM mode

Part Number: DRV8353


Hi 

We designed a motor drive circuit with drv8353s.

1xPWM mode is used for motor driving.

When DRV is disable(sleep mode), motor can be spined easy by hand.

However when DRV is enable(active) and the referance PWM signal is not be implemented to DRV,  motor is aligned and spinning the motor is more difficult.

We checked SHx pins. SHx pins are connected to GND. According to datasheet  SHx pins must be HiZ or  Not Connected. 

How can we get SHx pins as NOT CONNECTED?