Hello,
A question concerning the two current protection modes on the DRV8332 device: If my understanding of the data sheet is correct, in CBC mode, the device will attempt to limit current and then latch off if it cannot - how does the device determine that it cannot limit the current, in other words, at what point does the 'second protection system', as the data sheet puts it, kick in?
Also, once the latch off has occurred in CBC mode, does the device enter the same state as if it had latched off in OCL mode, i.e. the RESET_x lines have to be pulled low to re-activate the device?
Cheers,
John.