Hello,
I want to connect one brusded DC motor on the DRV8426x (x=E or P).
what is the best solution?
Do not use the second bridge in the IC or connect the second bridge in parallel with the first?
Best Regards.
Sylvain
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to connect one brusded DC motor on the DRV8426x (x=E or P).
what is the best solution?
Do not use the second bridge in the IC or connect the second bridge in parallel with the first?
Best Regards.
Sylvain
Is it allowed to connect the second bridge in parallel with the first to increase output current?
Best regards.
Sylvain
Sylvain,
This could cause a shoot-thru event as the timing to switch the two parallel connected bridges are not synchronized. If you need more current, please consider the DRV8256E or DRV8256P.
https://www.ti.com/product/DRV8256?keyMatch=DRV8256
Regards,
Ryan