hello team,my DC motor driver can drive and the functions(forward,backwards,slow,fast) are well but if I put a small load on it(improve the current slowly)it can run on 3A+ current but if I give it full pwm and hold the motor,the motor doesn`t have force (if I let it go it could keep going) i didn`t open the OCP this is my schematic .thank you !