I have a motor with dedicated 1:40 gearbox. But the motor shaft's bearing is mounted on the housing of the gearbox. So, I can't remove the gearbox. Is it ok to do the MPET while the gearbox attached?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a motor with dedicated 1:40 gearbox. But the motor shaft's bearing is mounted on the housing of the gearbox. So, I can't remove the gearbox. Is it ok to do the MPET while the gearbox attached?
Hi Robert,
Yes, it is okay to run MPET with gearbox. Please make sure the MPET open loop current is sufficient enough to drive the load during Ke measurement.
Regards,
Vishnu