What kind of tolerance should one expect with a given dead time setting in the OCP register? For example, if 100 ns is selected, would we expect it to be within 20% (80ns - 120 ns)?
Since the total dead time will be dependent on the FET VGS response in addition to the programmed dead time, is there an recommended method to measure just the programmed dead time?