Other Parts Discussed in Thread: MCF8316A
I removed R9 (22 ohm) from the component side and populated L1 on the backside with a 47 uH inductor (with 2.5 ohms series resistance). What is the recommended nominal value of series resistance for best operation?
Powering the EVM by connecting between VBAT and PGND, with Vm=12.0, the measured supply current was reduced from 35 ma (R9 populated) to 24 ma (L1 populated). This includes about 3ma when D1 and D4 are lit. Do these values seem reasonable (datasheet shows lower values)?
Using the GUI, by selecting BUCK power sequencing is disabled (BUCK_PS_SEQ_DIS), I was able to set the BUCK output (FB_BK) to 3.3, 4.0, 5.0, or 5.7 volts. It looks like the Datasheet functional block diagram below, shows FB_BK is the input voltage to DVDD LDO which regulates the power for the microcontroller?