Other Parts Discussed in Thread: DRV8801, DRV8873-Q1
Hi Team,
There is a good new that Customer is searching TI solution
The customer originally used the DRV8801, but the specification changed to a working voltage of 7~18V. Is DRV8872-Q1 a suitable choice for this project?
And the maximum motor current is 550mA, so the Motor Driver only needs to be >1A or more
1.Please suggest a best solution
2.Please provide comparison table and I will propose to customer ,THX