This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L-Q1: DIAG_RESULT bit

Part Number: DRV2605L-Q1

Hi,

I have same problem.

when ı use ERM, DIAG_RESULT bit working correctly  but if ı use LRA dont

I am taking "1" value from DIAG_RESULT bit after calibration mode and Diagnostic mode , always

LRA:   DM LM1040F- A

0.6Vrms

162Hz

12±2Ohm

2.55V

thank you,