Hi
Please recommend suitable products to replace PT5619
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
DRV8300 is a valid P2P replacement for PT5619 for both TSSOP-20 and 24-QFN packages. See below.
TSSOP-20
24-QFN
Thanks,
Aaron
Yes Gareth,
It is a bootstrap architecture gate driver that steps PWM inputs into VCC-level gate drive outputs for 6 N-type power MOSFETs.
DRV8300 supports up to 110-V abs max and -22V abs min on the motor phase pins and 125V abs-max on bootstrap pins. It also integrates bootstrap diodes and provides up to 1.5A gate drive current.
24-QFN package provides a MODE pin to support inverting and non-inverting PWM outputs, and DT pin which allows for adjustable driver dead time between 200 to 2000ns rather than PT5619 which supports fixed dead time of 500ns.
Thanks,
Aaron