Part Number: DRV8313
Would it be ok to connect all of nSLEEP, nRESET and nFAULT together, to an MCU weak pullup high to enable and the nFAULT can still pull low to indicate a fault?
Breaking the question down into 3 stages:
1. Tie nSLEEP & nRESET together
2. Connect nSLEEP & nRESET to nFAULT
3. Tie all 3 signals to MCU with weak pullup
-3.1 MCU will pull all 3 signals high (when there is no fault)
- 3.2 nFAULT's 10mA capability will pull MCU's GPIO + Weak pullup to logic low during fault
Notes:
nFault is OD with 10mA
MCU GPIO is weak pull up ~0.1mA equivalent