Hi,
I'm currently interrested in DRV8432 motor driver.
I saw you sell an Evaluation board and I have a question about mode select pin.
In the datasheet, it's specified at page 18:
"Mode select pins (M1, M2, and M3) should be connected to either VREG (for logic high) or AGND for logic low. It
is not recommended to connect mode pins to board ground if 1-Ω resistor is used between AGND and GND."
But on the DRV8432EVM Motor Drive Evaluation Board, mode select pin are connected directly to GND.
What about the recommendation?