Hi support team.
From the information posted below, it was found that the switch set by BUCK_PIS_DS at startup is connected to the VM.
On the other hand, the datasheet states that the circuit of the buck regulator is necessary even if the buck regulator is not used.

I recognized that the buck regulator is the source power of AVDD at startup, so I thought that the buck regulator need to configure components.
However the source power of AVDD at startup is VM, so I don't think the buck regulator is needed.
In case of the buck regulator is unused, why do I need to configure compornents.
Best regards,
Higa
Higa