Other Parts Discussed in Thread: L293D
Hello team,
My customer is facing an issue during ESSENTIAL CONTROLS on GUIDED TUNING SETTINGS.
<Issue>
Motor does not spin through I2C control.
Motor spin a few seconds through the potentiometer. Then motor stops and nFault LED turns on.
<Situation>
- GUI can perform "Read All Resisters". So the connection between GUI and EVM should be OK.
- When nFault LED turns on, GUI does not display the result on "FAULT STATUS".
- Even if "Auto read motor status" and "Auto read fault status" are disable, the situation is not changed.
- The customer is using the latest GUI on TI.com. And I placed order of the EVM on 05/09/2022 by TI.com. The customer is using the EVM board.
Please let me know if you need more information.
Best regards,
Shotaro