This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: TSD bit

Part Number: MCF8316A

Hi! 

When I run the motor, suddenly the TSD bit is set, together with the DRIVER_FAULT bit.

Only, according to the datasheet if an overtemperature happens, the OT bit should also be set. 

I also measured that the charge pump is still enabled, while according to chapter 7.3.22.10, the chargepump (with others) are disabled. 

In the image above, all faults are displayed. 

Thanks for any response!

Marcel