Hello Motor Driver Team!
I would like to use the DRV8328D in 3 PWM mode to drive a 12V / 10A peak bdc motor. I have 2x PWM pins available to drive the motor, so I am planning connecting the inputs as shown:
INL1 : HIGH
INH1: LOW / PWM
INL2: HIGH
INH2: PWM / LOW
INL3: LOW
INH3: NC (ok to float?)
Is there any issue in leaving one of the 1/2 bridges high z like this?