Hi,
in the Datasheet the Table 7-2 shows Resistors for current limits down to 7.4A.
The maximum Rating of the DRV8312:
"DRV8312 (Power Pad Down): up to 3.5-A Continuous Phase Current (6.5-A Peak)"
The Resistor maximum Rating is 200kΩ
Are the current Ratings for the DRV8312 experimental only? Or do i miss an Equation or Table?
Thanks in advance
Malte