Hi,
We got questions from our customers and would appreciate it if you could answer them.
The data sheet shows the min / max values for ΔItrip over the entire temperature range.
1. Is this "prone to max value in a high temperature environment" or "prone to max value in low temperature"?
2. Is it possible to provide normal distribution data for the measured output current values (300mA if possible) for multiple Lots?
Best Regards,
Nishie