Other Parts Discussed in Thread: MCF8316A
Hello,
I'm having trouble getting a motor to spin using the MCF8316AEVM. D1 and D4 are both green, ALARM and FAULT LEDs are both off. I have SW1 in the RUN position, S2 in the ABC direction, and S3 in the ON position. I have 24V connected to VBAT. As I turn the potentiometer counter-clockwise, the motor never spins. Algorithm State as shown in the GUI is always MOTOR_IDLE. I'm sure I'm missing something simple.
Thanks for the help.