Hi Team,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The TMP814 Variable Speed Single-phase Full-wave Fan Motor Predriver is “compatible with 12-V, 24-V, and 48-V Power Supplies.” Do we have a similar chip compatible with 110-V? Will chip settings be independent of a “CMOS battery?”
Thank you.
Regards,
May
Hello May!
Thanks for reaching out to us. Before I suggest a chip, do you mean 110V nominal operating voltage or 110V absolute maximum? We have options for 110V abs max applications (50-70V nominal applications) but we do not offer any ICs for 110V nominal systems.
Any additional information on the application/end equipment would help us determine what IC to recommend.
Please feel free to reach out with any further questions,
Tyler McCulloch