This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8245H-Q1EVM: nFAULT state when on power

Part Number: DRV8245H-Q1EVM


Hi team,

I am connecting the DRV8245H-Q1EVM with an external MCU. So I have removed all the 0 ohm resistor in area 1. I am trying the independent mode, so I gave nSLEEP, IN1 3.3V voltage and IN2, DRVOFF 0V as the datasheet says. But when i gave the VM, the nFAULT light (D2) stays on and the ic in sleep mode. Can you help me figure out what the problem is?

By the way, the VM is 10V which is stable, the 3.3V on ic is stable too. The out1 connect to a 8 ohm resistor, the out 2 connect to a 20 ohm resistor.

Thanks!

Best Regards

Daoming