This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8343-Q1: Enable functionality an Device configuration

Part Number: DRV8343-Q1

Hello,

we use the Part with SPI- Interface.
During my tests i does the following:

Device was powered (VM = 24 V) and enable pin = 1, the device was configured to 3x PWM Mode

After pulling the enable pin to low (0), and after a while to 1 again, the configuration of the device was lost and i had to reconfigure the device.

I serached the datasheet about this behaviour but i cound't find some answer.

My question:

Is the device configuration lost if the enable pin is low (longer than tRST, e.g 1 s) and than back to high?

best regards,
Steffen Müller