This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8812: Driving DRV8812 with a PWM Signal

Part Number: DRV8812


Hello,

I wanted to confirm something about the DRV8812, and any other GPIO Logic Motor Controller. I understand that when the enable pin is HIGH, then the motor runs at 100% PWM. Would it be possible, and acceptable to send a PWM signal to the Enable pin to allow for PWM control of the motor driver?