This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8702-Q1: Current closed loop

Part Number: DRV8702-Q1


Dear team,

Can our device support hardware current closed loop? If so, what is the accuracy?

Can our device support software current closed loop? If so, what is the accuracy?

Thanks & Best Regards,

Sherry

  • Can our device support hardware current closed loop? If so, what is the accuracy?

    Please see following section in the datasheet.

    7.3.4 Current Regulation

    Vio and Av tolerance are given in the datasheet electrical characteristics section.  Also contributing to error is the external shunt resistor.  

    Can our device support software current closed loop? If so, what is the accuracy?

    Please see section 7.3.5.

    Again, Vio, Av and external shunt tolerance contribute to error on SO.  SO can be used to externally close the loop on current.

    Regards,

    Ryan