Hello
iam trying to connect voice coil motor VM3850RB-200 to motor driver DRV2511Q1EVM.
Please advice,
1) If the connection can be made between them ? if yes how?
2)if not, please suggest any other motor driver ic that can be used with VM3850RB-200 .
2)Please give a simplified schematic .
VM3850RB-200 specifications:
voltage = 14.7 V
Current = 0.58 A
R = 25.4 ohm