hi TI member
--when using DRV8300 in motor control ,
sometimes we found the high side MOS and low side MOS turn short at the same time ,the bus line current may larger than 200Amps (I guess)
power supply is a Lithium battery pack;
check as follows , Q5 and Q6 short --------- Drain 、source、Gate are all short between each other;
--DRV8300 itself has the dead time protection , so in which condition , will cause the above case , i can't figure out it ,
we didn't do any restrict in our software ,pls get that
plz help
Thanks~~~
plz