Other Parts Discussed in Thread: DRV8706S-Q1EVM, UCC25600
Hi,
I'm currently doing an automotive new design and I have some concerns regarding the DRV8106-Q1. I was wondering if someone faced the same issues and could help me with that.
My application is driving a dc motor . I want to control it using an H-bridge and the DRV8106-Q1. My questions are the followings
1. Why don’t I see the transformer in the h-bridge of the schematic design of the DRV8706S-Q1EVM ? I want to use the DRV8106-Q1 in a half bridge topology and thus boost the input voltage from 12V to 24V so If this controller does not take the add of a transformer in the bridge this would not fit my application.
2.Can I program the chip with an eval board? Is there an internal eeprom in the controller, does it keep its configuration, or It has to be programmed at every power up?
3.Assuming I do not need the functionalities that come with the SPI, does the DRV8106-Q1 needs to be programmed at all or in that run with its raw internal circuits?
Thanks a lot guys !!