Hi team
Customer encountered some strange case on DRV8860, for some devices, when it's no-load, the DOUT has no output. The schematic is as below, the actual pull-up resistor is 270kohm. Do you have any insight? Thanks!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Customer encountered some strange case on DRV8860, for some devices, when it's no-load, the DOUT has no output. The schematic is as below, the actual pull-up resistor is 270kohm. Do you have any insight? Thanks!

Hi Shaofeng,
Are they seeing any data in DOUT of previous devices in the chain? or only at the DOUT of last DRV?
What is the value of VCC?
DOUT is being measured after which type of command? All available commands listed below.

Regards,
Pablo Armet
Hi Pablo
The DOUT will stop at the middle DRV8860, like U11 or U12 in the schematic. It's random case. The DOUT is no signal whatever the type of command.
Hi Shaofeng,
What is the VCC voltage? I am asking because the DRV8860 comes with an internal 1.4kΩ pull-up resistor to 5.7V. If external pull-up is different, there will be a conflict of voltage at the DOUT pin.
The DOUT will stop at the middle DRV8860, like U11 or U12 in the schematic. It's random case. The DOUT is no signal whatever the type of command
So the place where DOUT stops occurs at random? Is it reproducible consistently? Is it seen in multiple boards? Does it function properly with load connected?
Regards,
Pablo Armet