This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316: When the NPOR bit is set and how to clear it

Guru 12050 points
Part Number: DRV8316

Hi,

After initializing the DRV8316 registers, when I read the IC_Status register, the NPOR bit was set to 1.

Q1.Please tell me when the NPOR bit is set.

Q2. Is there any problem in operation even if the NPOR bit is set?

Q3.Is there a way to clear the NPOR bit? Setting the CLR_FLT bit in Control_Register_2 to 1 did not clear the NPOR bit.

Thanks,
Astro