Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625EVM-CT: Windows 11 support

Part Number: DRV2625EVM-CT

Do any of the haptic motor eval kits have support for Windows 11? 

When I attempted to use the DRV2625EVM-CT, the Haptic Control Console 1.6.0.2 crashes when I press 'connect'. I see from a different forum post that I would need Windows 7 to connect with DRV2625EVM-CT. Are there any other haptic driver eval kits which will actually work with the Haptic Control Console on Windows 11? 

  • After changing the properties of the Haptic Control Console 1.6.0.2 EXE to have win 7 compatibility mode, the program still crashed. However, this time, the Windows troubleshooter appeared for me. After selecting that the program worked previously in Win 7, the troubleshooter changed something, and now the program works for me.