This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8910-Q1: Differences of DRV89XX

Part Number: DRV8910-Q1

Hello!

What are the differences between the DRV8910 and DRV8908 except for the number of channels?

Not only DRV8908 have less bonding wire, are the chips different?

What are the differences between the DRV8908 and DRV8906 except for the number of channels?

DRV8906 have less bonding wire but are the chips same?

When using these with the same footprint, I want to consider which parts should be used for the reliability test of the unit.

Regards,