Hi TI
When using DRV11873 to start the brushless motor, the following three situations are encountered (we need the motor to rotate counterclockwise):
① Extreme situation: it rotates clockwise all the time;
② Common situations: clockwise rotation at intervals (clockwise rotation - stop - clockwise - stop...);
[The maximum instantaneous clockwise rotation speed shall not exceed 150rpm]
③ Occasional situation: stop and rotate counterclockwise (turn and stop, the speed is extremely low, visible to the naked eye)
Preliminary analysis of starting process: once the equipment obtains PWM signal, it will start the motor with 100% duty cycle until sufficient BEMF is generated (4 zero crossings are required); Once this happens, the device will enter the closed-loop control and enter the command speed according to the PWM input.
Question:
1. Why does the motor chip always rotate clockwise after acquiring PWM signal? What might be the cause? How do we debug through hardware or software?
2. Once the PWM signal is obtained, can the motor be started without 100% duty cycle and with low duty cycle? What parameters need to be adjusted?
Please analyze the above, thank you
The circuit schematic diagram is as follows: