Other Parts Discussed in Thread: , DRV8424
Hello,
The datasheet mentions that 3.3V logic levels are supported but I don't see any mention of how to support those logic levels. The datasheet says the Vih ranges from 1.5V to 5.5V so I'm assuming that value is dependent on an external reference rail somehow.
The DRV8256EEVM dev board looks like it ties an MSP430 3.3V logic signal directly to the EN pins and other logic level pins and there doesn't seem to be anything providing an external rail to the chip. However, the eval board uses a DRV8424 with software and hardware configurations to emulate operation of a DRV8256 so I'm not sure if that's a reliable source.
What should I do to ensure that I can drive the PH and EN pins with 3.3V logic levels?
VM in my application is 12V.
Thanks,
Ken