This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8860: Does the DRV8860PWR have locked rotor detection and diagnostic detection?

Part Number: DRV8860
Other Parts Discussed in Thread: DRV8873

Does the DRV8860PWR have locked rotor detection and diagnostic detection?


Is the over-current protection and detection in this material related to locked rotor?


If it does not meet the requirements of locked rotor detection and diagnostic detection, are there any other recommendations for similar specifications

  • Hello,

    All the protection is defined in the datasheet in section 8.3.3.  There is OCP, but that is meant for output shorts.  

    What type of motor are you trying to drive and current rating?  We have some devices like the DRV8873 with iPropi output that can give you current information.  As current increases, would indicate a stall.  

    Regards,

    Ryan