Other Parts Discussed in Thread: DRV8834
Hi Experts,
Good day.
The customer is using DRV8835 implements the related micro-stepping control PWM signals but the motor rotation isn't smooth and the motor force is weak. Below is the DRV8835 output signals with and without load/motor.
Without Load With Load

About the implemented micro-stepping - it's 1/8 with a PWM frequency of 16.6kHz.
Can you tell me if is it possible to use somehow micro-stepping with DRV8835?
We need noiseless motor rotation and smooth current waveforms.
Keep safe.
Regards,
Josel