Other Parts Discussed in Thread: DRV8353
STM32G474+DRV8353R is used to control the PMSM, with the PWM frequency of 40K. When the power supply voltage is below 50V, the motor will operate normally, and the power supply voltage exceeds 55V, the speed will increase correspondingly, but the DRV will be burned. May I ask what the following reasons are?