This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8803: Can DRV8803 support 200kHz switching rates when used as general DO in PLC?

Part Number: DRV8803

I only find "Motor speed can be controlled with pulse-width modulation at frequencies from 0 kHz to 100 kHz." in DRV8803's datasheet.

I want to use DRV8803 as a Low-Side Switch in my design, the switching rates needs to be 200KHz.

Can DRV8803 support that? Or is there any other IC recommended?