The three pins of electric PIN24/25/26 are connected to GND. R55 and R57 are both 200m Ω. The voltage of PIN12 and PIN13 is 1V. The supply voltage, also the voltage of PIN4 and PIN11, is 24V.
Now, the problem is that after the circuit board is powered on, the DIV and STEP pins are suspended. If the EN pin is enabled, the 24V power supply has 200mA current, the motor does not rotate, and the DRV8825 heats seriously. If the motor is disconnected, the input current of 24V voltage is almost 0. Is this normal?In this case, if the STEP input signal is provided, the 24V voltage and current is about 400mA, the motor operates normally, and the DRV8825 is still severely overheated.