This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316A: Buck converter unused

Part Number: MCT8316A

Hi,

I really do not have any use of the internal buck converter but the FB_BK pin provides power to the internal DVDD voltage regulator so I at least need a supply voltage there. Is it OK to connect the external 3.3V_logic power we already have in the design to the FB_BK pin? Then, by setting the Buck regulator to 3.3V I assume it will be idle and produce no error states.

Regards

Goran Ekstrom

Apodosis AB