Will this motor driver run at a "fixed speed" WITHOUT an MCU? I want to apply power and have the motor automatically run at 3500 RPM until power is removed. The speed would remain at 3500 regardless of load or supply voltage as long as the current is below 8A peak.