This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8328: Using DRV8328 for single phase motor

Part Number: DRV8328


Hello,

I'm 99% confident I can use this part for a single phase BLDC motor but I just wanted to ask the question so I don't make an expensive mistake.

Can I do this?

My approach would be to use the INHA and INHB inputs (3x PWM input version) to drive two of the half bridges which I would combine into an H-bridge configuration.

For INHC and INLC, I would just tie them to ground so that GHC/GLC are kept low and SHC would be high-z.

Is it ok to leave GHC/GLC floating in this configuration?

Are there other considerations that I need to account for such as inadvertently triggering one of the protective circuits?