Other Parts Discussed in Thread: DRV8876, , DRV8872
I was trying to do simulation for DRV8876 in LTspice giving inputs at IN1 and IN2.Whatever the input condition is I am only getting high on OUT1 and OUT2 pins. I have tried the following conditions
1) IN1 High and IN2 Low
2)IN1 Low and IN1 High
3)IN1 and IN2 PWM with 100kHz duty
Vm 12V is given
Vref 3.3V
Pmode is given high
Imode is grounded with 30k
Iprop is grounded with 1500ohms.
Please correct me if anything I have done wrong