This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8424: Control Signals and Inputs for DRV8424PPWPR

Part Number: DRV8424
Other Parts Discussed in Thread: DRV8256, ,

Hello Team,

We are using DRV8424PPWPR to drive the stepper motor. I have four signals coming from FPGA namely,

1. Enable,

2. Step,

3. PWMIN1

4. PWMIN2.

For this DRV8424PPWPR devie we have four inputs namely,

1. AIN1

2. AIN2

3. BIN1

4. BIN2. 

I want to connect four control signals to these four inputs. As DRV8424PPWPR doesn't have separete enable and step inputs, from EVK user guide I got some understadings which are as below. Kindly refer the attached image for more clarity. Let me know if my understanding is correct.

Understandings I had,

1.From this above table can we assume AIN1 can be used as Enable pin irrespective of DRV8424P, DRV8424E, DRV8256 etc and as well as PWM input,

2.BIN1 can be used as STEP pin irrespective of DRV8424P, DRV8424E, DRV8256 etc and as well as PWM input,

3.AIN2 can be used to control Direction and can be used as DIR pin irrespective of DRV8424P, DRV8424E, DRV8256 etc and as well as PWM input.

Regards,

Vikas H

  • Vikas,

    Any reason you can't consider the DRV8424 that has a STEP/DIR interface and would allow you to easily hookup to your FPGA and only need two pins?  STEP and DIR (this could be connected to any GPIO).

    Regards,

    Ryan