This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8876: PSPICE model and simulation of the current limiting function

Part Number: DRV8876


Hello,

I am trying to use the PSPICE simulation model of the DRV8876 for current limiting/regulation purpose. See my schematic below:

So whatever the value of the resistor installed on the IPROPI, I cannot change the current limit or regulation value. With the actual schematic, the current value is around 1.5 A again whatever the resistor:

So can you tell me if the PSPICE model is good for that purpose or evaluation?

Thank you

Regards

Bruno