Other Parts Discussed in Thread: UC2625,
The circuit follows Voltage control mode of UC2625. The RPM of the motor keeps increasing over a period of time from the desired RPM. lets say intented RPM is 4900 but after a duration of 10 min the RPM will be 5100 and keeps increasing. we subjected the UC2625-EP to a higher temperature to 80°C. The RPM increases tremendously upto 300+ counts and reverts back during cooling phase. All other components in the PCB are thermally isolated from the UC2625-EP. Only the UC2625-EP was subjected to high temperature whereas remaining all the components at its ambient temperature 24°C. kindly post your options to resolve the issue. Thanks