dear
I have two questions about Offline Short Circuit and Open Load Detection.
1. For example, if the pull-up current source and resistor R are connected in series between VDD and GND, how to calculate the voltage of the current source.
2. Can you give an example of how to configure the current source combination and how to determine whether it is open load or short circuit according to the VDS status? Assume that VDS_LVL and EN_OLSC are configured correctly.
thanks in advance